Specify the Output Format

Use the Output Format field on the SQL Export tab to specify the format in which Geo SCADA Expert is to export the result of the SQL Query.


Choose from:

Further Information

Specify the Character Set used to Encode the Exported SQL Query Result.


Disclaimer

Geo SCADA Expert 2019