Conditions.bool-factor

A single boolean factor preceeded with an optional NOT

Format

[ NOT ] { ( bool-condition ) |

bool-primary-comparison |

bool-primary-between |

bool-primary-in |

bool-primary-like |

bool-primary-like-regex |

bool-primary-isnull |

bool-primary-exists |

bool-primary-unique }

[ IS [ NOT ] { TRUE | FALSE | UNKNOWN } ]

Remarks

A bool-factor is an expression the result of which is True, False, or Unknown. A bool-factor can be any one of:


Disclaimer

Geo SCADA Expert 2019