Expressions
            This section describes the syntax of scalar expressions.
Contents
| Name | Description | 
|---|---|
| Case expression | A function selecting a value conditionally | 
| expr-column-ref | 
                                 A reference to a column in an expression. A column might comprise another expression, or a reference to a database field.  | 
                        
| expression | One or more expression terms separated by addition and/or subtract operators | 
| expr-factor | A single value | 
| expr-primary-cast | Converts a value from one type to another | 
| expr-primary-constant | A constant keyword | 
| expr-primary-datetime | A date, time or timestamp value | 
| expr-primary-element | Extracts one element from a string of delimiter separated elements | 
| expr-primary-format | Returns a string formatted according to instructions contained in a format String expression. | 
| expr-primary-interval | An interval value | 
| expr-primary-location | A location function that allows you to specify location values. | 
| expr-primary-odbc-datetime | A date, time or timestamp value | 
| expr-primary-odbc-function | An ODBC function | 
| expr-primary-odbc-timestampadd | Adds a number of specified intervals to a timestamp | 
| expr-primary-odbc-timestampdiff | Returns the difference between two timestamps | 
| expr-primary-opc-time | An OPC relative time | 
| expr-primary-sumfunc | An aggregate function returning a summary of data returned in a query | 
| expr-term | One or more expression factors separated by multiply, divide or concatenate operators | 
| Numeric value function | A function returning a numeric value | 
| String value function | A function returning a string value |