Index Columns

An Indexed Column is a column in the database that can be accessed more quickly than other columns (there are internal mechanisms that allow these columns to be searched more easily than the other columns).

There are a limited number of Index Columns, and the Index Columns that are available vary according to the type of table that is being searched. The following table shows the Index Columns that are available for each type of database table:

Table Type

Unique Indices

Non-Unique Indices

Object

Id, FullName

ParentGroupId, Search Keys

Aggregate

-

Id

Alarm Condition

-

Id

Event Journal

RecordId

Id, Source, FileId

Point Historic

RecordId

Id

Processed Historic

RecordId

Id

Forecast Historic

RecordId

Id

Data Table

-

As configured

Data Grid

-

-

Data Set - -
Alarm Summary

ActiveTime

InactiveTime

-

The columns are listed in cost order, for example, for the Object table, the Id column has a lower cost than the FullName column (and so can be searched more efficiently than the FullName column).

The values in the rows of an Index Column are referred to as index values.


Disclaimer

Geo SCADA Expert 2019