Scalar Literals

Scalar literals are used to represent constant values in expressions and search conditions within an SQL command or query. The following types of literal are supported:

Type Description
String

A sequence of characters enclosed in single quotes. A single quote character is itself represented by two immediately adjacent single quote characters.

Examples:

'' 'Some Text' 'Don''t stop'

Integer

Written as a signed or unsigned integer number.

Examples:

0 65535 -50

Real

Written as a floating point number.

Examples:

0.5 100.0 5.75E-4 -2.5E12

Bit String

Written either as sequence of 0s and 1s, or as a sequence of hexadecimal digits.

Examples:

B'1010110111' X'3CF8'

All numeric values in SQL use the English decimal point (a dot).


Disclaimer

Geo SCADA Expert 2019