Debug Mode

You can use Debug mode to access the various debugging options. Debug mode is enabled when you:

  1. Display a Mimic in Run mode (see Run Mode and Design Mode in the Geo SCADA Expert Guide to Mimics).
  2. Select Debug Mode in the View command group on the Graphics tab.

Or:

  1. Display a Mimic in Design mode.
  2. Select Edit Script in the View command group on the Graphics tab.
  3. Deselect the Design Mode button on the Quick Access Toolbar.

Or:

  1. Display the Script Editor for a Mimic.
  2. Deselect the Design Mode button on the Quick Access Toolbar.

Or:

  1. Display an Alarm Banner script (see Display the Global Script Editor).
  2. Select Debug Mode in the Debug command group on the Script tab.

While in Debug Mode, the ViewX ribbon displays the Script tab. The Script tab includes debugging options in the Debug, Breakpoints and View command groups.

The Debug group contains commands that allow you to Debug a Script.

The Breakpoints group contains commands that allow you to use breakpoints while debugging (see Debug a Script).

The View group contains commands that display additional debugging tools.

The debugger operates in one of three states:

The current state is displayed on a status bar that appears at the top of a script while it is in Debug mode.


Disclaimer

Geo SCADA Expert 2019