Mimic.Navigate

The Mimic.Navigate function allows the script to open a defined display in the current window

Syntax

Mimic.Navigate(URL)

Description

Opens a defined display in the current window.

Arguments

URL {string}

The address of the display that is to be opened. The URL has to use the Geo SCADA Expert address format.

Returns

String

Example:

Mimic.Navigate("SCX:////CMimic/Overview Mimic")

When run, this script causes a Mimic named 'Overview Mimic' to be displayed in the current window, replacing the Mimic that contained the script.

For more information, see Hyperlink to Another Display.

Take care not to confuse the Mimic.Navigate function (which is a function of the Mimic object) with the Mimic_Navigate function. The Mimic_Navigate function is an event handler function and varies according to the language in which you are coding.


Disclaimer

Geo SCADA Expert 2019