Slider.Maximum

The Slider.Maximum property is used to set the highest value for the slider.

Syntax

Slider.Maximum = HighestValue

Description

Defines the highest value on the slider.

Arguments

HighestValue {integer}.

Defines the highest value that can be selected on the slider.

Returns

None.

Example:

Slider.Maximum = 250

This sets the slider range so that it ends at 250. There are no slider positions higher than 250.


Disclaimer

Geo SCADA Expert 2019