Slider.TickFrequency

The Slider.TickFrequency property is used to define the number of ticks on the slider.

Syntax

Slider.TickFrequency = TickValue

Description

Defines the frequency of ticks on the slider.

Arguments

TickValue {integer}.

Defines the frequency of ticks on the slider. For example, if the Minimum is 0 and the Maximum is 100 and you set the TickValue to 10, the entire range of values for the slider is divided into 10 sections, with each section marked by a tick.

Returns

None.

Example:

Slider.Minimum = 0

Slider.Maximum = 100

Slider.TickFrequency = 10

This sets the slider range so that it begins at 0 and ends at 100. The entire range is divided into 10 sections with each section marked by a tick.


Disclaimer

Geo SCADA Expert 2019