System

The System function allows DOS commands to be issued from the script,

Syntax

System (Command)

Description

Issues a DOS command from the script.

Arguments

Command {string}

This is a DOS command.

Returns

None.

Example:

System ("ping 192.168.0.117")

This pings the IP address 192.168.0.117.


Disclaimer

Geo SCADA Expert 2019