Create a Password Blacklist item

To create and configure an item in the database, you need to be logged on via a User Account that:

To implement the use of a password blacklist in Geo SCADA Expert you must first create a Windows based (not UNIX or Mac) ASCII or UTF-8 source text file that contains the list of words that you want to blacklist, with one word per line followed by a carriage return.

A sample password blacklist source file is provided and located in following directory:

C:\Program Files\Schneider Electric\ClearSCADA\Samples

When you have created the source blacklist file you can continue to create a password blacklist item in Geo SCADA Expert.

  1. Display the Database Bar (see Display an Explorer Bar).
  2. In the Database Bar, right-click on the Group, or Group Template within which you want to add a blacklist item.
    A context-sensitive menu is displayed.

    Although you can create more than one Password Blacklist item, you can only actively use one.

  3. Select the Create New option
    A further menu is displayed.
  4. Select the Password Blacklist option from the Security menu.
  5. Give the password blacklist a suitable name (see Naming Restrictions).
  6. When the item is ready you can import the password blacklist source file.

Disclaimer

Geo SCADA Expert 2019