Define the Certificates Settings for Original WebX Clients

ATTENTION: This section and associated topics apply to the Original WebX client only.

To help protect your system against unauthorized access, Geo SCADA Expert uses certificates for Original WebX clients.

The certificates allow the Geo SCADA Expert server to use encryption for client-server communications.

There are two types of certificates that Geo SCADA Expert can use for Original WebX. The certificates must be in PEM or DER format.

If a server generated non-trusted SSL certificate is used, the client will display warning messages when users access the system. The exact warning message depends on the browsers, but typically might be "There is a problem with this website’s security certificate". Some users may find these warning messages distracting, although they do not affect their ability to interact with your Geo SCADA Expert system.

If a trusted SSL certificate is used, the client is able to verify that it is connecting to the expected server, and so there are no warning messages shown when a client accesses the secure web server ports.

We recommend that you purchase trusted SSL certificates for your web servers so that users do not receive distracting warning messages. We also recommend you review your security options and establish appropriate security for your web server.

Recommended security:

Maximum security:

Not recommended:


Disclaimer

Geo SCADA Expert 2019