Define the Home Page Settings for a User

The properties described in this topic apply both to User Forms and User Pattern Forms. (User Patterns only apply to systems on which Geo SCADA Expert can create new User accounts automatically as part of an External Authentication process. For more information, see Create User Accounts from a User Pattern.)

You can associate a 'home page' Mimic or Trend with each user account. The home page item that is associated with a user’s account is displayed whenever:

The home page for Guest ViewX client user is defined on the General tab of the Options window (see ViewX Options in the Geo SCADA Expert Guide to Client Administration). The home page for Guest web client users using the Original WebX client is defined as the 'Default View' on the Group tab of the System Form (right-click on a system item (Root Group), then select Edit Properties to display the Form).

To define the 'home page' settings:

  1. Either:

  2. Select the General tab.
  3. Select the browse button next to the Home Page field to display a Reference browse window. Select an appropriate 'home page' display from the window. You can choose any Mimic or Trend.

  4. Select the ViewX tab.
  5. In the General section, use the Show Home Page at Logon check box to define whether the 'home page' is displayed automatically whenever the user logs on via a ViewX client:

    Select the check box for the home page to display automatically when a user logs on to a ViewX client via the account

    Clear the check box if the home page is not to display automatically when a user logs on to a ViewX client via the account.

    (Providing that a Home Page is specified for the user account, that Home Page will display automatically whenever the user logs on via a Virtual ViewX client, regardless of the setting of the Show Home Page at Logon check box.)


Disclaimer

Geo SCADA Expert 2019