Define the User Location Sources

The properties described in this topic apply both to User Forms and User Pattern Forms. (User Patterns only apply to systems on which Geo SCADA Expert can create new User accounts automatically as part of an External Authentication process. For more information, see Create User Accounts from a User Pattern.)

Geo SCADA Expert clients can regularly report location information to the Geo SCADA Expert server. This can be useful if you want to track users and determine their proximity to database items (such as outstations). Alarms can then be redirected appropriately. To use this functionality, set the location Source to Dynamic on the user's Location tab (see Use the Location Tab to Specify an Item's Geographic Coordinates in the Geo SCADA Expert Guide to Geographical Location Support):

The following types of client can report location information to the server:

A client can report the following information to the server:

ViewX and Virtual ViewX clients update their location information to the server when the user logs in. Mobile clients update the server as a result of a change in location. All clients will update the server no more than once a minute. Geo SCADA Expert does not direct alarms to clients that are not logged in.

To specify which clients you want to update the server with location information:

  1. Either:

  2. Select the General tab and scroll down to the User Location Sources check boxes.

  3. Define the User Location Sources settings for the user account.
    • Select the check boxes for the clients that you want to update the server with location information.
    • Clear the check boxes for the clients that you don't want to update the server with location information.

Disclaimer

Geo SCADA Expert 2019