Define which Operational Features are Available to a User in Original WebX

The properties on the WebX tab of User Forms and User Pattern Forms apply purely to Original WebX. To configure settings for ViewX and Virtual ViewX clients, you use the properties on the ViewX tab of the User Form or User Pattern Form (whichever is applicable to your system setup).

The properties described in this topic apply both to User Forms and User Pattern Forms. (User Patterns only apply to systems on which Geo SCADA Expert can create new User accounts automatically as part of an External Authentication process. For more information, see Create User Accounts from a User Pattern.)

Use the Operational section of the WebX tab to define which operational features are available when the user logs on from an Original WebX client. The section only lists operational features that you can set independently to those that apply when the user logs on via either a ViewX or Original WebX client. For information about defining features that apply to ViewX, Virtual ViewX and Original WebX, see Define the General Settings that Apply to ViewX and Virtual ViewX.

To define which operational features apply when the user logs on via an Original WebX client, rather than a ViewX client:

  1. Either:

  2. Select the WebX tab.
  3. Define the Operational settings:

    • Operate—Select this check box if the user is allowed to execute methods (perform actions) on items in the database. For example, select this check box if the user is to have access to actions such as Control and Acknowledge Alarms. Remember that the User Account has to have appropriate security permissions for the database items in addition to having this check box enabled on the User Form. For example, for a User Account to provide Original WebX access to the alarms for a database item, the User Account has to be assigned the View Alarms permission for that database item and have the View Alarms check box selected on the User Form. Additionally, for the user to have access to the Acknowledge Alarms action, the User Account also has to be assigned the Acknowledge Alarms permission for that database item.

      Clear the check box if the user is not to execute such methods. Access to context-sensitive menus displayed by selecting items in the Database Bar will be restricted to pick actions (as opposed to methods). For example, to pick actions such as Notes and Display Current Trend.

      NOTICE

      UNEXPECTED BEHAVIOR OF APPLICATION

      Clearing the Operate check box has no effect on the methods that a user can access from displays that use ActiveX controls, such as Mimics, Queries Lists, Events Lists, and Alarms Lists. To prevent access to methods on such displays, use other security measures, such as restricting the user's Original WebX access to such displays, or restricting access to such methods on a User, User Group, database Group or database item basis.
      Failure to follow these instructions can result in unexpected user activity.
  4. Save the configuration.

Further Information

Allocating Security Permissions.

Define whether a User can view Alarms, Alarm Summary data, and Events Lists via ViewX and Virtual ViewX clients: see Define the General Settings that Apply to ViewX and Virtual ViewX.

Define a User's Operator Document Store: see Define the General Settings that Apply to ViewX and Virtual ViewX.


Disclaimer

Geo SCADA Expert 2019