Export a Password Blacklist
Geo SCADA Expert provides you with the facility to export the password blacklist that is contained within a Password Blacklist item. This allows you to retrieve the list in the event the original source file has not been archived.
To export a password blacklist:
- Display the Database Bar (see Display an Explorer Bar).
- In the Database Bar, right-click on the password blacklist item from which you want to export a password blacklist.
A context-sensitive menu is displayed. - The Export password blacklist dialog is displayed:
This allows you to enter the location and the filename of the exported password blacklist or you can use the browse button to search for a location to save the file.
- Select OK to save the file. Geo SCADA Expert creates a Windows based ASCII text file containing the blacklist.