Using the Default, Non-Trusted Certificate

ATTENTION: This section and associated topics apply to the Original WebX client only.

We recommend that you purchase a trusted certificate for use with Original WebX, as trusted certificates offer better protection against unauthorized system access. However, it is possible to use the non-trusted certificate that is generated automatically by Geo SCADA Expert.

NOTICE

SECURITY THREAT

Using a non-trusted certificate could compromise your system security. Installing a non-trusted certificate could compromise your system security. Potentially, it could lead to unauthorized access. For this reason, we strongly recommend that you use a trusted certificate.
Failure to follow these instructions can result in equipment damage.

Non-trusted certificates should only be used if a trusted certificate is not available and your business network is secure. (Although we still recommend that you use trusted certificates, even with secure networks).

If you use a non-trusted certificate, logging on via a Original WebX clients will result in:

Or:


Disclaimer

Geo SCADA Expert 2019