Define the Driver Request Timeouts

This section applies to advanced drivers only.

You can use the Geo SCADA Expert Server Configuration Tool to define the maximum amount of time permitted for a driver to complete a request. By defining a maximum time, you allow the driver to abort a request that is taking too long to complete.

There are two driver request timeouts:

Typically, the default settings of 10 minutes, with a 5 minute extension are adequate. However, certain requests such as a file transfer or download configuration may take longer due to slow communication links, or very large files or outstations. For these types of request, you may need to increase the timeouts.

Requests that are aborted due to a timeout are logged in the Event Journal.

Some drivers have their own timeout that is used instead of the Request Timeout (for specific requests that routinely take longer to complete). For more information, please refer to the relevant Driver Guide).

To define the limits for the two request timeouts:

  1. Access the Geo SCADA Expert Server Configuration Tool (see Accessing the Geo SCADA Expert Server Configuration Tool).
  2. Expand the Global Parameters branch of the tree-structure.
  3. Select Drivers.
  4. In the Timeouts part of the Drivers section configure the following fields:
  5. Request Timeout

    This allows you to define the maximum amount of time permitted to perform a request. If the request is still pending at the end of this time, the driver detects that the request has failed and aborts the request.

    Request Timeout Extension

    This allows you to define the additional amount of time permitted for an active request to complete. If the active request does not complete within the defined time, the driver detects that the request has failed and aborts the request.

  6. Right-click on the system icon in the tree-structure, and select the Apply Changes option to apply the changes.
  7. Restart the required driver(s) so that the new timeout(s) take effect (main server only). For more information, see Start and Stop a Driver.
  8. Repeat steps 2-6 inclusive for the other servers in the system, except permanent standby servers.

Disclaimer

Geo SCADA Expert 2019