Define the Type of Value that is Stored in a Standard Custom Field

When you add an extra field, you need to specify the type of value that can be stored in the field so that it is appropriate for your requirements. To do this, you need to use the Type setting on the Edit Field window.

To access the Edit Field window, see Add or Modify an Extra Field.

When you have displayed the Edit Field window, use the Type setting to choose the data type for the field:

When you have defined the Type setting, you can continue to define the other field settings as required.


Disclaimer

Geo SCADA Expert 2019