Define where an Extra Field is Shown on Queries Lists

You can use the Edit Field window to define whether an extra field is included in Queries Lists, and if so, where its column is shown on the Lists. To do this, you need to display the Edit Field window (see Add or Modify an Extra Field) and then use the List Priority setting:

When you have defined the List Priority, you can continue to define the other field settings as required.


Disclaimer

Geo SCADA Expert 2019