Example: Isolated Main (Arbitrate)

This example describes the sequence of events that would occur when a Main server in a multi-server architecture becomes isolated (see Define what Action Should be Taken when a Server Becomes Isolated). In this case, the network connection has been lost and ICMP polls have failed.

The network consists of a Hot-Standby Pair. Server A is the Main server and Server B is a Standby server.

The settings for both servers are as follows:

The sequence of events is as follows:

  1. The network connection is lost. Server A is isolated. Server A remains the Main server and Server B becomes a Main server so that it can function independently.

  2. The network connection is restored. There are now two Main servers.

  3. Arbitration takes place to determine which server will now be the Main server and which will be the Standby server (see Define the Server’s Arbitration Priority). If Server A were to win arbitration, Server A would remain the Main server and Server B would become the Standby server.

Further Information

Hot-Standby Pair Architecture


Disclaimer

Geo SCADA Expert 2019