Historic Data Storage Settings

The Historic Data settings apply to the historic data for database items that support historic data storage (database points, master station accumulators and some driver-specific items). This differs from event data and configuration changes data (see Historic and Archive Data). When enabled, the Historic Data feature creates historic files, with each historic file containing 1 week's worth of historic data for an individual item.

Do not confuse the Historic Data settings with the Historic Files setting. The Historic Files setting allows you to enable or disable historic storage of reports and documents, for example, file upload reports and Crystal Reports reports (see Enable or Disable Historic Files).

The Historic Data settings are located in the Historic Configuration branch of the Server Configuration Tool:

Historic Data Settings (Server Configuration Tool)

You can use the Historic Data settings to:

Further Information

Define the Acceptable Limits for Historic Data Files


Disclaimer

Geo SCADA Expert 2019