Modify a Historic View

You can edit an existing Historic View so that it:

Editing a Historic View allows you to make amendments to a Historic View (for example, change a Historic View from calculating an average value to calculating a total value), or to use an existing Historic View's configuration as the basis of a new Historic View.

To edit an existing Historic View:

  1. Access the Geo SCADA Expert Server Configuration Tool.
  2. Expand the SQL Query Configuration branch.
  3. Select Historic Views.

  4. Right-click on the Historic View that you want to edit from the list of historic views.
    A context-sensitive menu is displayed.

  5. Select the Modify option.

  6. Use the Modify Historic View window to alter the settings. The various fields and combo boxes work in the same way as the corresponding settings on the Add Historic View window.

    ATTENTION: Any SQL queries that use the previous name of the Historic View will need to be updated with the new name, otherwise they will no longer operate.

    Take care with End and End Last Historic Algorithms used on clients, or with Geo SCADA Expert features, that run in Local Time with Daylight Saving Time. Ensure that the start and end times specified for the sample interval do not coincide exactly with the time at which the clock jumps backward. Include a small offset in the sample time, to offset the calculation to avoid the sample end or start time exactly matching the time that the clock jumps backward at the transition from Daylight Saving Time to Standard Time. A small offset of 1s or even 1ms should suffice. For more information about Daylight Saving Time, see The Effects of Daylight Saving Time Adjustments.

  7. Select the OK button to close the Historic View Properties window.
  8. Right-click on the system icon in the tree-structure, and select the Apply Changes option to apply the changes.

Now that you have modified a historic view, you can either proceed to configure other Historic settings (see Historic Configuration Settings) or you can continue with the server configuration.


Disclaimer

Geo SCADA Expert 2019