Modify an ODBC Table Link

If you need to change the configuration of an existing ODBC Table Link:

  1. Access the Geo SCADA Expert Server Configuration Tool (see Accessing the Geo SCADA Expert Server Configuration Tool)
  2. Expand the SQL Query Configuration branch.
  3. Select the Linked ODBC Tables branch to display the Linked ODBC Tables section.
  4. Right-click on the link that you want to edit, and then select Modify from the context sensitive menu.
    The Modify Linked ODBC Table window is displayed.
  5. Use the settings on the Modify Linked ODBC Table window to change the configuration of the link. The settings work in exactly the same way as the corresponding settings on the Add Linked ODBC Table window (see Create a Link between an External ODBC Database and Geo SCADA Expert)
  6. Select the OK button to confirm your selections and close the Add Linked ODBC Table window.
    The new linked table configuration is now in place.
  7. Right-click on the system icon in the tree-structure, and select the Apply Changes option to apply the changes.

Disclaimer

Geo SCADA Expert 2019