Removing a Point State Alarm

If you want to delete a point state alarm:

  1. Display the Geo SCADA Expert Server Configuration Tool (see Accessing the Geo SCADA Expert Server Configuration Tool).
  2. Expand the Database Configuration branch.
  3. Select the Point State Alarms branch.
  4. In the Point State Alarms section, double-click on the Table entry for the relevant type of point table. Each table represents a type of database point. There are descriptions for each table—use the description to determine which table is used for the type of point that is to use the point state alarms.
  5. When you double-click on a table, the Point State Alarm Conditions window is displayed.
  6. Select the name of the point state alarm that you want to remove.
  7. Select the Remove button.
  8. Repeat steps 4 to 6 inclusive for each point state alarm for the selected type of points.
  9. Select the OK button to confirm the selection and close the Point State Alarm Conditions window.
  10. Repeat this procedure for each point state alarm that you want to remove.

Disclaimer

Geo SCADA Expert 2019