TCP/IP Connection Problems

Problems with the TCP/IP network connection between the Geo SCADA Expert servers and the remote computer are displayed in the Events List and they are also displayed as alarms on the various alarm displays.

For more information on possible messages, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

If no messages are displayed, the communication failure may be due to Serial Connection Problems.


Disclaimer

Geo SCADA Expert 2019