Welcome to the Server Administration Guide

Intended Audience

This guide is designed for use by system administrators who are responsible for setting up and managing the Geo SCADA Expert system.

Document Scope

This guide primarily explains how to use the Server Configuration Tool. Available on Geo SCADA Expert servers, the Server Configuration Tool contains a variety of settings that have a system-wide effect, including:

The Server Administration Guide also describes administration-related features of the Geo SCADA Expert Server Status Tool, and how to use other Geo SCADA Expert administration utilities.

Server Configuration Tool

 

The Geo SCADA Expert Server Configuration Tool is designed to be used by administrator level users. We regard server administrators as high level users that have knowledge of some configuration tasks as well as installing Geo SCADA Expert and setting up the Geo SCADA Expert servers. These users should understand the system setup and server arrangements.

If you are unfamiliar with the server configuration process, we recommend that you complete each section of the Server Administration Guide in turn so that you learn about the available features. Before you begin, you should familiarize yourself with the information on Operating Systems and Operational Limitations - Server, in the Geo SCADA Expert Installation Guide.

When you are ready to configure your Geo SCADA Expert server, you can use the Partners settings to set up the server arrangement. For more information, please refer to the relevant section in System Architectures:

If you are familiar with the server configuration process, you can refer to the section that describes the settings for which you require information. A list of the settings and the corresponding sections is included in Understanding the Geo SCADA Expert Server Configuration Tool.

If you are familiar with the layout of the Server Configuration Tool, you can go directly to the section that describes the relevant settings or feature. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.


Disclaimer

Geo SCADA Expert 2019