Alarm Redirections

The Alarm Redirections category provides status information for any alarm redirections that are in process.

WARNING

ALARM NOTIFICATIONS DURING SHUTDOWN

If the server is shut down while alarm redirections are in process, the pending alarm redirections will be lost. On lone server systems, this means that the intended recipients will not be notified. On multi-server systems, the alarm redirections will still be sent to the recipients, but from the Standby server that goes Main.
On a lone server system, the loss of pending alarm redirections can result in death, serious injury, or equipment damage.

The alarm redirection status information is categorized as:


Disclaimer

Geo SCADA Expert 2019