Clients (WebX)

The WebX branch of the Server Status Tool includes a Clients category. The Clients category provides status information about each Original WebX client that is connected to the server.

The status information for each Original WebX client is categorized under these headings:

The number of clients varies according to the size of your system.

The Clients (WebX) category is often used to check that Original WebX clients have valid licenses (they will be unable to connect to the server if they have invalid licenses) and also to determine which Original WebX clients have a connection to the server.

Further Information

Original WebX Status Information.


Disclaimer

Geo SCADA Expert 2019