Get Support for a Specific Driver

Geo SCADA Expert supports many different drivers, including popular telemetry drivers such as DNP3, IEC 60870-5, and Modbus. You can view the drivers that are installed on your system by using the Modules status information (see Modules). You can also use the Modules section to access the support details for each driver. To access the support details, your computer needs access to the Internet.

To access the Support feature:

  1. Display the Modules status information in the Server Status Window (see Modules).
  2. From the list of drivers that are installed, right-click on the driver for which you require assistance.
  3. Select the Support option from the context-sensitive menu.
    The relevant online support page is displayed (providing that your computer has access to the Internet).

Further Information

Schneider Electric technical support details available from the About dialog box in ViewX: see Check the Version of your Geo SCADA Expert Software.

Find Updates for a Specific Driver

Access Documentation for a Specific Driver.


Disclaimer

Geo SCADA Expert 2019