Locks

The Locks category provides status information about the software locks. Typically, you will only need to view the lock status when asked to do so by Schneider Electric engineers—the engineers may use the status information to diagnose performance issues such as latency.

For diagnostic information regarding database locks in Geo SCADA Expert, see Lock Diagnostics Read and Lock Diagnostics Write. The Locks category displays all locks within the server, whereas database locks are specific to the 'database' and assist in identifying which operation is causing high lock utilization.

The status information for each lock is categorized as:


Disclaimer

Geo SCADA Expert 2019