Polls

In multiple server systems such as Hot-Standby systems, each server monitors the other servers (up to 2 other servers). You can use the Polls category to see whether the server on which you are working can access the other server(s) and if so, what state it deems the other server(s) to be in. This is useful for checking that the Main and Standby servers can communicate with each other correctly and are able to arbitrate the correct Main and Standby status.

The information that is shown in the Polls category is used by the server as part of the Main-Standby arbitration process.

The standby polls status information is categorized as:


Disclaimer

Geo SCADA Expert 2019