Define Whether a Scanner is Used to Trigger Logic

The scanners on many simple drivers can be used to trigger logic programs within Geo SCADA Expert. Where this feature is supported, you can use the Always Update on Scan check box to define whether the scanner is to be used in this way. The check box is displayed on the Scanner tab of the Scanner Form:


Disclaimer

Geo SCADA Expert 2019