Operational Limitations - Client

Geo SCADA Expert has a number of recommended operational limits. Expansion beyond the recommended limits is possible, but may result in a system that is unstable and unreliable. The recommended operational limits for Geo SCADA Expert clients are:

Parameter

32-Bit Limit

64-Bit Limit

Notes

Minimum ViewX to Geo SCADA Expert server link bandwidth

2 Mbit

2 Mbit

Exceeding these limits will cause slow performance in ViewX.

Maximum ViewX to Geo SCADA Expert server link latency

150 ms

150 ms

Exceeding these limits will cause slow performance in ViewX.

Minimum Virtual ViewX client to Virtual ViewX server link bandwidth

1 Mbit

1 Mbit

 
Minimum Original WebX client to Geo SCADA Expert server link bandwidth

2 Mbit

2 Mbit

 

For information on server operational limitations, please see Operational Limitations - Server.


Disclaimer

Geo SCADA Expert 2019