Typical Install
If you choose Typical on the Choose Setup Type ‘page’, you are presented with three options:
Select this option to install the most commonly used server and client components. These include Geo SCADA Expert server, ViewX Client, WebX Client (for Original WebX), and Data Access components.
The typical Server and Clients installation contains the same components as the Full Install.
Select this option to install the ViewX Client (including the Aquis client, and the Crystal Reports component if the 32-bit Crystal Reports runtime prerequisite has been installed), WebX Client (for Original WebX), and Data Access. These are the most commonly used client components.
Select this option if you only want to install the WebX client and Data Access components (which allow Web, OPC, OLEDB, ODBC, and COM connections). ViewX and Geo SCADA Expert server components are not installed when you select this option.
If you select Server and Clients, the Geo SCADA Expert Installer displays the Custom Setup ‘page’ (see Custom Setup).
If you select Clients or Data Access, the Geo SCADA Expert Installer displays the Ready to Install ‘page’ (see Ready to Install).
The