Log On to ViewX

To configure the database items required for Geo SCADA Expert to communicate with a SCADAPack Modbus controller, you need to log on to ViewX via a user account with Configure permissions. The preconfigured 'EngExample' user account has sufficient permissions to perform the tasks in this section, so if you are not already logged on as 'EngExample', you need to do so (see Log on to your System).

Once you are logged on as the 'EngExample' user, you can proceed to Create a 'Serial Comms' Group and a 'Site' Group.

Further Information

Logging On and Off: see System Security.


Disclaimer

Geo SCADA Expert 2019