Test Your Knowledge on the ViewX Interface

Do you know your way around the ViewX interface? Can you display Explorer Bars, browse to database items and navigate between ViewX windows with ease? Then put your ViewX skills to the test and see how much you have learned:

  1. What is the main display area in ViewX called?
  2. How do you expand a Group so that you can see its contents?
  3. Group folders are represented by white folder icons, but what do the red and green folder icons represent?
  4. If you need to display the configuration Form of a database point, which Explorer Bar would you use to locate the point, and then display its Form?
  5. You are viewing a Mimic in the Document Display Area and then choose to display a configuration Form. When it is displayed, the Form fills the available space so that you can’t see the Mimic any more. How can you switch ViewX’s focus from the Form back to the Mimic?
  6. If you wanted to know which database item is associated with an alarm, which two columns of information would you look at on the Alarm Banner?
  7. How do you inform Geo SCADA Expert (and other users) that you have seen an alarm and are in the process of investigating its cause?

Disclaimer

Geo SCADA Expert 2019