Sampling Tables

Use a Sampling Table to collect periodic values from a register (tag) on a TBox RTU. Sampling tables are available only on Analog points.

The values are collected at regular intervals or on an external trigger (this is configured on the RTU). A tag may be configured with more than one Sampling Table. A single Sampling Table is a sequence of one of the following values, calculated over a specified period:

Sampling tables are typically used to capture data on values that change slowly over time, for example, water flow.

A single TBox outstation can have up to 64 sampling tables, and the tables can hold data of type BYTE, WORD or INT. The recording period can be from 1 second to 12 hours, and can also be triggered externally.

Data in a sampling table is not timestamped, but the time of the most recent value is recorded .

A sampling table is distinct from a Sampling Tables. Chronologies are collected on the occurrence of events, typically large changes in a value. You can include both Chronologies and Sampling Tables in a Trend.

In Geo SCADA Expert, in order to retrieve a Sampling Table of instantaneous values, you configure the Analog Point as for a Chronology (see Chronologies).

For other Sampling Tables (minimum, maximum, mean or incremental) you need to:

  1. Configure a TBox Outstation to correspond to the TBox RTU (see Configuring a TBox Outstation).
  2. Create a TBox Historical Analog Point.
  3. Associate the Historical Analog Point with the parent Analog Point that matches the TBox tag for which you want to retrieve the sampling table (see Configuring TBox Historical Analog Points).
  4. Configure the Historical Analog Point (see Configuring TBox Historical Analog Points).
  5. Enable historic data logging on the Historic tab of the Historical Analog Point Form (see Defining Historic Details for a Point in the Geo SCADA Expert Guide to Core Point Configuration).
  6. Select Logged Data in the Historic Data Filter property on the Analog Point tab (see Configuring TBox Analog Points).
  7. Specify the interval for retrieving historical data from the outstation (see Define the TBox Properties).

Disclaimer

Geo SCADA Expert 2019