Scanner Methods

A Totalflow Scanner object supports the following object-specific methods, some of which are also available as pick actions from ViewX and Virtual ViewX:

This method is also available as a pick action. As such, if your user account has the relevant permissions, you can right-click on a Totalflow Scanner object in the Database Bar, and then select the Change Gas Composition pick action. The Change Gas Composition window is displayed.

The parameters that you need to specify are listed in the table below. The parameters are listed in the order in which they need to appear in the method call. Use the App Number field to specify the number of the Application in the Totalflow for which you want to change the gas composition.

Select the Live Composition check box to change the Live Analysis Data in the Totalflow device, instead of the Fixed Analysis Data.

If you select the Normalize option, the non-zero gas composition values are adjusted in equal proportion so that so that the sum of all of the elements equals 100. The method call/pick action will be unsuccessful if the individual gas composition values do not sum to 100 and the Normalize option is not selected.

The driver does not automatically update the points that monitor the gas composition after the ChangeGasComp method is called. You will either need to call the Refresh method on the Totalflow Scanner, or wait for the next poll for points to be updated.

Parameter Name

Number

Fixed
Array.Index
Live
Array.Index

Type

Unit

App Number

1

 

 

byte

none

Live Composition

2

 

 

bool

none

N2 nitrogen

3

3.21

3.46

double

percent

CO2 carbon dioxide

4

3.22

3.47

double

percent

H2S Hydrogen Sulfide

5

3.23

3.48

double

percent

H2O Water

6

3.24

3.49

double

percent

He Helium

7

3.25

3.50

double

percent

CH4 Methane

8

3.26

3.51

double

percent

C2H6 Ethane

9

3.27

3.52

double

percent

C3H8 Propane

10

3.28

3.53

double

percent

C4H10 n-Butane

11

3.29

3.54

double

percent

C4H10 i-Butane

12

3.30

3.55

double

percent

C5H12 n-Pentane

13

3.31

3.56

double

percent

C5H12 i-Pentane

14

3.32

3.57

double

percent

C6H14 n-Hexane

15

3.33

3.58

double

percent

C7H16 n-Heptane

16

3.34

3.59

double

percent

C8H18 n-Octane

17

3.35

3.60

double

percent

C9H20 n-Nonane

18

3.36

3.61

double

percent

C10H22 n-Decane

19

3.37

3.62

double

percent

O2 Oxygen

20

3.38

3.63

double

percent

CO Carbon Monoxide

21

3.39

3.64

double

percent

H2 Hydrogen

22

3.40

3.65

double

percent

Ar Argon

23

3.41

3.66

double

percent

Normalize

24

 

 

bool

N/A

Further Information

Scanner Data Fields


Disclaimer

Geo SCADA Expert 2019