Totalflow Numeric Point

Use a Totalflow Numeric Point object can be used to read and write (control) any value from a Totalflow that is specified by an Application, Array and Register that holds a numeric value. The specific formats that are supported are shown in the table below:

Type Name

Size in Bytes

Range

Description

BYTE

1

0 to 255

An 8 bit unsigned integer

INT16

2

-32768 to 32767

A 16 bit signed integer

INT32

4

-2 147 483 648 to
2 147 483 647

A 32 bit signed integer

UINT16

2

0 to 65535

A 16 bit unsigned integer

UINT32

4

0 to 4 294 967 296

A 32 bit unsigned integer

FLOAT

4

Valid single precision float

A single precision floating point value

The Totalflow Numeric point can read System Application Registers that have a type of ‘Byte’ (as defined in the Totalflow XSeries Flow Computer Manual).

If a value pointed to by an App/Array/Register has an Access of Read/Write, the value can be written to by calling the Control Method on the Control aggregate on the point.

Further Information

Numeric Point Configuration


Disclaimer

Geo SCADA Expert 2019