Why are the points that read gas composition not updated when the ChangeGasComp method is executed?
When the ChangeGasComp method is called on the Totalflow Scanner, the driver task gets a read only collection of points that are attached to the scanner. As the references are read only, their values cannot be updated during the method call.
NOTE: You do not actually need to have points that read the gas composition to call the ChangeGasComp method.