Delete a Y-Axis

Each Trend can display multiple Y-Axes as required. If you need to remove a Y-Axis from a Trend:

  1. Display the Trend that has the Y-Axis that you want to remove (see Display a Trend in Design Mode).
  2. Right-click on the Y-Axis that you want to remove.
    A context sensitive menu is displayed.
  3. Select Delete.
    The selected Y-Axis is removed from the Trend display.
  4. Save the configuration.

Any traces that use the deleted Y-Axis are also removed from the Trend when you delete that Y-Axis. For this reason, you should assign traces to a Y-Axis that will remain on the Trend (see Configure a Trace).


Disclaimer

Geo SCADA Expert 2019