Display the Full Scale on a Y-Axis

If you have changed the zoom of the Y-Axis of a Trend, you can use the Full Scale option to redisplay the entire Y-Axis scale.

To display the full scale on a Y-Axis:

  1. Right-click on the Y-Axis.
    A context sensitive menu is displayed.
  2. Select Full Scale.
    The Trend will display the entire Y-Axis.

Disclaimer

Geo SCADA Expert 2019