Pan a Trend

You can also use the Pan tool to force the Trend to show data plotted before or after the currently displayed interval. This is useful as it allows you to view data between two set intervals. For example, if the X-Axis shows one hour from 09.25 to 10.25, the Previous Interval and Next Interval tools only allow you to view 08.25-09.25 and 10.25-11.25 respectively. By using the Pan tool, you can view any hour’s worth of data, for example, you could pan the Trend so that it displays values for the time period 09.55 to 10.55.

To use the Pan tool on a Trend:

  1. Display a Trend in Run Mode.
  2. Either:
    1. Right-click in the main display area on the Trend.
      A context sensitive menu is displayed.
    2. Select Pan.
      The cursor changes to a hand with a pointing fingerPointing Cursorthis indicates that Pan mode is active.

    Or:

    • Select the Pan Mode command from the Navigation group on the ribbon's Home tab.
  3. Position the cursor over the main display area of the Trend.
  4. Press the left-hand mouse button. Keep the button pressed down.
  5. Drag the Trend to the left until the required time and values are displayed.
  6. Release the left-hand mouse button.
    The Trend pans to the selected time.

To turn Pan mode off, repeat step 2 of the procedure above. If Pan mode is already active, selecting the Pan button or option toggles Pan mode to off.


Disclaimer

Geo SCADA Expert 2019