Trend Key

The Key is displayed at the bottom of the Trend display. It lists the traces that are shown on the Trend and provides information about the source of the trace (its values, category, and so on).

Trend Key

Each row of the Key provides information for one of the traces on the Trend. By default, the key displays information in four columns: Trace, Type, Ruler Value, and Axis. If your User account has the Configure permission for the Trend, you can use the Columns feature to display different or additional columns (see Define the Columns on the Key).

The predefined columns that can be displayed in the key include:


Disclaimer

Geo SCADA Expert 2019