XAXIS Mandatory Value

The XAXIS section in a TrendSpec definition has to have one mandatory value, <X-Axis Mode>.

Mandatory Value Type XAXIS Mandatory Values
Comments

<X-Axis Mode>

Identifier value

Use to define the type of time scale used for the x-axis.

Specify one of these values:

Absolute, RelativeNow, or RelativeLatest.

(For information on each type of x-axis mode, see Configure the X-Axis.)

Example:

RelativeLatest
(For an ad hoc Trend that displays data for a time that is relative to the latest value to be plotted on the Trend.)

If required, you can specify one or more XAXIS Optional Values after the above mandatory value.


Disclaimer

Geo SCADA Expert 2019