Configure the Trio Diagnostics Digital Point Properties

D Series radios provide support for interrogation of fewer diagnostics parameters than other supported radio series. To retrieve an item of diagnostics data from a D Series radio, you associate that data with a Trio Diagnostics Analog Point; other types of point are not used to retrieve diagnostics data from D Series radios.

Use the fields on the Trio Diagnostics tab to configure a digital point’s Trio Diagnostics specific properties. Some of the fields are common to many Trio Diagnostics points (see Configure the Common Trio Diagnostics Point Properties). Fields that are specific to Simple Trio Diagnostics Digital points are explained below.



Disclaimer

Geo SCADA Expert 2019