Geo SCADA Expert Client

Geo SCADA Expert clients are programs that run on the computers that access the Geo SCADA Expert database (the Geo SCADA Expert database is stored on the Geo SCADA Expert Server). The Geo SCADA Expert clients communicate with the Geo SCADA Expert server via a network connection.

You can operate Geo SCADA Expert via a ViewX Client or a Virtual ViewX Client. Geo SCADA Expert also supports other methods of accessing its data, for example, via Microsoft® Excel or Crystal Reports.

Typically, you need to log on to a Geo SCADA Expert client before you can work with your system. You log on by entering a unique user identification name and a password. These details are associated with a user account that allows you entry to the system, along with permissions that determine which features and database items you can access.

Depending on the permissions that have been allocated to your user account, you might be able to:

When you perform an action (or ‘method’), the relevant instruction is sent to the Geo SCADA Expert server, where it is processed. The action is then either performed within the Geo SCADA Expert server or is sent to the relevant outstation or other device (depending on the type of action).

If an outstation receives a control (from an action), it processes the data and then sends an instruction to the instruments that operate the plant—for example, a signal to start a pump.


Disclaimer

Geo SCADA Expert 2019