OPC Data Bar

The OPC Data Bar is an Explorer Bar (see Explorer Bars). The Bar uses a hierarchical ‘tree’ structure (see Working with Explorer Bars) to allow you to browse the various OPC properties in the database.

The OPC Data Bar is a useful tool for higher levels users for building and configuring the Geo SCADA Expert system, configuring Mimics and Trends, debugging the system, or when connecting other systems to the database. For more information, see Working with the OPC Data Bar.


Disclaimer

Geo SCADA Expert 2019