Accepting Local Configuration Changes

If you change the configuration of a Field Device locally, the Field Device will signal Geo SCADA Expert. The signal is used by Geo SCADA Expert to alert users that the configuration in the Field Device may be different to the corresponding configuration in Geo SCADA Expert. The alert can be presented as:

 

If the local configuration has been changed, you can:

If you make and accept local changes to the incremental configuration, you may later decide to discard these changes. To do this, you will need to download all configuration from Geo SCADA Expert, and not just any changes made in Geo SCADA Expert. You can only remove all of the local changes by downloading all configuration.

If you make local changes but do not accept them, and then download only configuration changes from Geo SCADA Expert, the entire incremental configuration is downloaded automatically. This operation is designed to remove the local changes.

If you make local changes to the bulk configuration, downloading only the configuration changes is sufficient to remove all of the local changes. This applies irrespective of whether you have accepted the local changes, as a bulk configuration file will be downloaded.


Disclaimer

Geo SCADA Expert 2019